Littelfuse Wins Consulting-Specifying Engineer's Product of the Year Silver Award
CHICAGO, September 23, 2013, - Littelfuse, Inc., the global leader in protection, control and sensing technologies, announced today, that it has won the Silver Award for the 2013 Consulting-Specifying Engineer Magazine (CSE) Product of the Year Awards for its EL3100 Ground-Fault & Phase-Voltage Indicator. This competition honors the best new products in the safety, HVAC, electrical and plumbing systems engineering markets. The EL3100 was chosen from more than 110 products that qualified as finalists for the competition.
The EL3100 Ground-Fault & Phase-Voltage Indicator is part of the Littelfuse Protection Relay line. It detects dangerous electrical conditions that can significantly damage equipment and harm employees. These relays can help identify problems in advance and prevent costly downtime and productivity loss.
"We are honored that Consulting-Specifying Engineer readers continue to select Littelfuse products as Product of the Year winners," says Dan Stanek, Vice President and General Manager of Littelfuse Protection Relay and Custom Electrical Products.
About the EL3100
The EL3100 is a self-powered ground-fault and phase-voltage indication system for 3-phase systems. It meets the National Electrical Code (NEC®) and the Canadian Electrical Code (CEC®) requirements for ground detectors for ungrounded alternating-current systems. Voltage connections are provided on the EL3100 for 208, 240, 480, and 600-V systems. Three green LED's on the EL3100 indicate the presence of phase-to-ground voltage and one red LED indicates a ground-fault. The EL3100 can operate stand-alone or with up to five remote LED indicators. The solid-state relay output provides indication of a ground fault.
For more information
For more information on Littelfuse Protection Relay Products visit the Littelfuse protection relay website at: www.littelfuse.com/relayscontrols or call our technical support line at 1-800-832-3873.
About Littelfuse
Founded in 1927, Littelfuse is the world leader in circuit protection with growing global platforms in power control and sensing. The company serves global customers in the electronics, automotive and industrial markets with technologies including fuses, semiconductors, polymers, ceramics, relays and sensors. Littelfuse has over 7,000 employees in more than 35 locations throughout the Americas, Europe and Asia. For more information, please visit the Littelfuse website: littelfuse.com.
LFUS-R
Media Contact:
Eva Jelezova
Marketing Manager, Protection Relays
Littelfuse, Inc.
Tel: 773-628-0706
ejelezova@littelfuse.com