News Details

View all news

New Line of Littelfuse 1500vdc Photovoltaic Fuses Protects Next Generation of Solar Equipment

June, 18, 2013

New Line of Littelfuse 1500vdc Photovoltaic Fuses Protects Next Generation of Solar Equipment

June 18, 2013 at 12:00 AM EDT
New Line of Littlefuse 1500vdc Photovoltaic Fuses Protects Next Generation of Solar Equipment

CHICAGO, June 17, 2013 -- Littelfuse, Inc., the global leader in circuit protection, today announced it has developed in cooperation with leading photovoltaic equipment providers a Series of 1500VDC photovoltaic fuses designed to protect the next generation of solar installations. The SPXV and SPXN Series of fuses meet the tough requirements of 30kA interrupt ratings, 1500VDC protection and global standards critical to solar equipment manufacturers.

The new SPXV series includes string protection fuses from 6 to 20 amps in a 10 x 85 mm design and slightly wider 25 and 30 amp fuses, designed to fit the same holders. The standardized size allows for maximum flexibility of array construction, as fuse rating is often a final step in specification. With eight products under 30 amps, Littelfuse offers the broadest selection of fuse options. All of the new string protection fuses fit into a new 1500V LPXV holder.

The higher amperage SPXN, with six models ranging from 200 amps to 400 amps, also comply with global standards, including UL2579 and IEC 60269-6. These products feature a ventilation-enhancing, cylindrical design, with sturdy melamine construction that meets the standard NH3L package size. The blade and bolt mounting feature provides flexibility in mounting and easy installation and replacement.

Both the high and low amperage models were specifically designed to minimize wattage loss and provide the highest efficiency product for 1500VDC installations. This not only improves long-term system cost; it also reduces internal cabinet temperatures.

"With our innovative new 1500 VDC product offering, we are well positioned to support the design leaders in the solar industry," stated Dan Gilman, Director of Global Sales. "Our work with major OEM partners and our application knowledge have enabled us to develop a 1500 VDC solution that meets global standards and also provides high levels of efficiency."

The 1500VDC SPX Series augments the SPF and SPFJ fuses for 1000VDC protection, as well as other photovoltaic protection products. Littelfuse is a leader in the solar market, providing a broad range of products and support for customers around the globe.

For more information about the new photovoltaic fuses from Littelfuse, visit us at Intersolar Hall B, stand 414or visit our website at littelfuse.com/solar.

About Littelfuse
Founded in 1927, Littelfuse is the world leader in circuit protection with growing global platforms in power control and sensing. The company serves customers in the electronics, automotive and industrial markets with technologies including fuses, semiconductors, polymers, ceramics, relays and sensors. Littelfuse has over 7,000 employees in more than 35 locations throughout the Americas, Europe and Asia. For more information, please visit the Littelfuse website: littelfuse.com.

LFUS-P

CONTACT:
Maureen Janosch
Marketing Manager
Littelfuse, Inc.
773-628-0718
mjanosch@littelfuse.com

Multimedia Files:

Categories: Press Releases
View all news
opens in new window