Low-Capacitance TVS Diode Array from Littelfuse Provides Clamping Voltages Over 50 Percent Lower than Similar Silicon Solutions

SP3014 Series Product Image
CHICAGO, September 8, 2014 Littelfuse, Inc., the global leader in circuit protection, has introduced the low-capacitance SP3014 Series TVS Diode Array (SPA® Diodes), to provide protection for electronic equipment that may experience destructive electrostatic discharges (ESD). The SP3014 Series, which integrates two channels of low capacitance steering diodes and a zener diode, can safely absorb repetitive ESD strikes above the maximum level specified in the IEC61000-4-2 international standard without performance degradation. The SP3014 Series provides clamping voltages more than 50 percent lower than similar silicon solutions to protect the most fragile ICs from damage or premature failure from electrical transients. Its low loading capacitance makes it ideal for protecting high-speed signal lines such as USB 2.0, USB 3.0, and 1Gb Ethernet. An extremely low dynamic resistance protects sensitive, state-of-the-art chipsets against damage or premature failure that may result from ESD by clamping the overvoltage transient to a safe level. Typical applications include ultrabooks, notebooks, LCD TVs, set-top boxes, Ethernet switches, external HDDs, smartphones, automotive electronics, etc.
"The SP3014 Series with its dynamic resistance of 0.04? offers circuit and hardware designers a highly optimized clamping device capable of protecting the most sensitive ICs against electrical transients such as ESD" said Chad Marak, director of the TVS Diode Arrays product line. Not only does the SP3014 offer the near ideal brick wall clamping response, but it also presents only 0.5pF of loading capacitance making it suitable in a multitude of low and high-speed applications.
The SP3014 Series TVS Diode Array offers these key benefits:
- Incredibly low dynamic resistance of 0.04Ω provides clamping voltages more than 50 percent lower than similar silicon solutions to protect even the most fragile ICs from damage or premature failure.
- Robust ESD capability of ±15kV (contact), ±25kV (air) allows manufacturers to claim ESD protection above the maximum level as stated in the IEC standard.
- Low capacitance of 0.5pF minimizes signal degradation to preserve system performance and reduces the designer's dependency on accurate trace impedance simulators.
- Small form factor μDFN-6L package simplifies the PCB layout by allowing the traces to run directly underneath the device without the need for stub traces that can cause signal degradation.
- Automotive-grade quality ensures maximum reliability in the harshest environments.
Availability
The SP3014 Series TVS Diode Array is available in quantities of 3,000 in tape and reel packaging. Sample requests can be placed through authorized Littelfuse distributors worldwide. For a listing of Littelfuse distributors, please visit Littelfuse.com.
For More Information
Additional information is available on the SP3014 product page and data sheet. If you have technical questions, please contact: Chad Marak, Product Director, cmarak@littelfuse.com.
About Littelfuse
Founded in 1927, Littelfuse is the world leader in circuit protection with growing global platforms in power control and sensing. The company serves global customers in the electronics, automotive and industrial markets with technologies including fuses, semiconductors, polymers, ceramics, relays and sensors. Littelfuse has over 8,000 employees in more than 35 locations throughout the Americas, Europe and Asia. For more information, please visit the Littelfuse website: littelfuse.com.
LFUS-P
Media Contact:
Rhonda Stratton
Global Marketing Communications Manager
Electronics Business Unit, Littelfuse, Inc.
773-628-0644
rstratton@littelfuse.com
https://twitter.com/littelfuse