Upgrades highlight safety and reliability of the device
CHICAGO--(BUSINESS WIRE)--
Littelfuse,
Inc., the global leader in circuit protection, today announced
product updates to the Industrial Shock-Block® SB6100, Special-Purpose
Ground-Fault Circuit-Interrupter (GFCI). Improvements to the Industrial
Shock-Block® SB6100 include:
-
The SB6100 Equipment Ground-Fault Protection Device (EGFPD) version
has flexible protection with adjustable trip settings at 6 mA and
from10 to 100 mA in increments of 10 mA to avoid nuisance tripping in
high-noise applications such as welding.
-
The SB6100 has an automatic self-test feature that ensures the unit is
operating properly.
-
The motor starter feature allows the user to start the motor from the
device interface.
-
Both SB6100 models (GFCI and EGFPD) are certified to CSA C22.2 No.
144-M91 Ground Fault Circuit Interrupters.
"According to OSHA, on average five workers are electrocuted weekly, and
electrocution is the cause for 12 percent of young worker deaths in the
workplace. With statistics such as these, it's increasingly important to
adopt safety devices like the SB6100 Industrial Shock-Block," says
Darrick Santa Maria, director of product management, Industrial Business
Unit at Littelfuse.
About the SB6100 Series Industrial Shock-Block®
The SB6100 Series Industrial Shock-Block® is a GFCI, which meets UL
943C. Until now, GFCIs have not been practical in industrial settings.
The SB6100 can be used on systems up to 600V and with much higher
leakage current than residential GFCI devices. The SB6100 is available
in a NEMA-4X UL-listed enclosure or as an open-chassis unit.
Applications for this product include electrical cabinets supplying
power to pumps, washers, mixers and other areas where operators,
electrical equipment and wet conditions are present.
Download high resolution image: http://www.littelfuse.com/~/media/protection-relays/press-image/isb_gfci.jpg
About Littelfuse
Founded in 1927, Littelfuse is the world leader in circuit protection
with growing global platforms in power control and sensing. The company
serves global customers in the electronics, automotive and industrial
markets with technologies including fuses, semiconductors, polymers,
ceramics, relays and sensors. Littelfuse has over 10,000 employees in
more than 40 locations throughout the Americas, Europe and Asia. For
more information, please visit the Littelfuse website: Littelfuse.com.
LFUS-P

View source version on businesswire.com: http://www.businesswire.com/news/home/20161003005261/en/
Debra Jayson
Commercial Marketing Manager
Industrial Business
Unit
Littelfuse, Inc.
773-628-0738
djayson@littelfuse.com
Source: Littelfuse
News Provided by Acquire Media